9/20/2017 2:23 PM | |
Posts: 2 Rating: (0) |
Hello, Does anyone have any experience in deploying Labview programs to a Panel PC running windows 10 IOT enterprise? As far as I am aware the Enterprise IOT version is as close as you can get to the desktop version. I have developed a few test programs on a development PC, and successfully deployed them to a touch screen panel pc using the iot applications builder, by building an exe with an installer. While the program is running, if the user opens the on screen keyboard, the Labview program then loses the ability to be minimized, and then restored. Once the program is minimized, it seems to get stuck in the task bar? You ARE able restore the program by starting task manager, finding the program, and clicking maximize. However, simply clicking the icon in the task bar refuses to restore the program. Does anyone have the same problem. Any help will be appreciated. thank you. |
9/20/2017 2:50 PM | |
Joined: 9/23/2005 Last visit: 4/26/2024 Posts: 4522 Rating: (698) |
Shouldn't you ask the NI Community ? |
Regards, |
|
Follow us on