6/27/2017 8:33 AM | |
Posts: 215 Rating:
|
Maybe this one, but I'm not sure. |
6/27/2017 11:39 AM | |
Posts: 215 Rating:
|
Firstly, I only talk about SIMATIC IOT2040. I'm not sure something like Simulink IOT even exists. Secondly, I apologize for my comments on the connection of IOT and Mindsphere. It should in theory be possible I guess, though I haven't seen an application example for this nor did I test such things. There are however other cloud platforms out there, for which there are already posted examples. For example, see this thread on connection to IBM bluemix, or this one on connection to Microsoft Azure |
6/28/2017 1:34 PM | |
Joined: 6/26/2017 Last visit: 7/19/2019 Posts: 5 Rating:
|
I'm sorry, I mixed up the terms SIMULINK and SIMATIC. Of course I'm talking about the SIMATIC IoT 2040. I'm mainly interested in the connection possibilities of the SIMATIC IoT 2040 with MindSphere. However, I will check the suggested links related to IBM bluemix and MS Azure as well. JDarius, thanks for providing these links! |
6/30/2017 10:46 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
There is no way to turn a "SIMATIC IOT2040" in a "MindConnect IoT2040"! The "MindConnect IoT2040" is a ready to use product with a proprietary operating system. It has an own MLFB (9AC2112-0AA00-1YA2). Here is the link to this product. The "SIMATIC IOT2040" (MLFB: 6ES7647-0AA00-1YA2) is just a piece of hardware where the user has to run an own OS or our Example Image. The only thing the two different products have together is the hardware (MindConnect IoT2040 uses the SIMATIC IOT2000 as hardware platform). I hope this makes things more clear Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
2 thankful Users |
7/3/2017 10:58 AM | |
Joined: 6/26/2017 Last visit: 7/19/2019 Posts: 5 Rating:
|
Bergmanu, thanks for clearing things up! |
8/3/2017 5:38 PM | |
Joined: 4/16/2015 Last visit: 4/3/2024 Posts: 45 Rating:
|
It's now possible to connect the SIMATIC IOT2040 to the MindSphere with the MindConnect Library. The MindConnect Library is a C/C++ based Library which allows you to connect the SIMATIC IOT2040 to the MindSphere. You need to program Connecting, Disconnecting, Buffering and Sending Mechanisms. A detailed tutorial how to do this is attached in the MindConnect Library Getting Started. In the first step only MindAccess Developer can download and use the MindConnect Library. So the MindConnect Library is for free, but to test it you need the MindAccess Developer in the first step. In further steps MindSphere will be more and more open so that MindAccess Developer won't be neccessary for pure connectivity anymore. That means in about half a year :-( the MindConnect Library will be free and usable without the Test Access. I have attached you a Document how to get started and a Link with MindSphere Documents. If we have tested the solution ourselfes over the next time we will put a more detailed tutorial in the IOT2000 Forum. AttachmentMindSphere_MindAccess_Developer_datasheet_en.pdf (437 Downloads) |
Last edited by: Philipp_ at: 8/3/2017 5:41:33 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on