4/28/2021 11:03 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, What was your problem with Modbus on node-red? For me this works fine. you could try to use the python Modbus module. Another option would be to use C/C++ with libmodbus. Therefor you would need to use our SDK for cross-compiling. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
4/30/2021 11:23 AM | |
Joined: 4/17/2018 Last visit: 8/28/2024 Posts: 86 Rating: (5) |
Find included two sample flows using the node-red-contrib-modbus library. The sample connects to an S7-1500 CPU running as Modbus TCP server. The ANxx sample shows some more code as examples. As always: No warranty given Attachmentsample_modbus_client_s7_helperFunctions_flow.zip (570 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on