8/18/2017 1:11 PM | |
Joined: 10/18/2012 Last visit: 12/15/2023 Posts: 225 Rating: (23) |
This LED indicates that your IPC is on and shows if the Watchdog is active. See Page chapter "1.2.2 Status displays" at page 16 of the Operating Instructions manual at https://support.industry.siemens.com/cs/ww/en/view/87514045. regards, |
This contribution was helpful to1 thankful Users |
8/24/2017 2:56 PM | |
Joined: 10/18/2012 Last visit: 12/15/2023 Posts: 225 Rating: (23) |
When you switch on the IPC - Is there anything on the screen? Maybe some light, or not even this? Did you try to connect an external screen via the DVI or DP Interface? Maybe you can open the IPC and check all components inside the IPC? Are all RAM-Modules tight connected to the motherboard? Is every cable on it's right place? If the problem still persists I would consider contacting the Technical Support at https://www.siemens.com/automation/support-request. regards |
This contribution was helpful to1 thankful Users |
Follow us on