Industry Online Support
Technical Forum
9/26/2011 10:38 PM | |
Posts: 22 Rating:
|
Is it acceptable to have an output before a function block, or do all outputs need to be at the end of each rung/network? For example: see attachment Splitted from Simple Beginner Question. |
Last edited by: O_Moderator at: 9/27/2011 12:14 PMnew subject after splitting Last edited by: O_Moderator at: 9/27/2011 8:16 AM |
|
9/27/2011 7:02 PM | |
Joined: 1/28/2009 Last visit: 9/25/2023 Posts: 6822 Rating:
|
Dear AutoNub In STEP7 you have option of using "---( # )--- Midline Output". Check the attachment of using this prior to call a FB.Also check the attachment for more detail on that which is extracted from the STEP7 online manual. Best regards Attachmentmid.zip (32 Downloads) |
Follow us on