1/11/2022 3:16 AM | |
Joined: 12/14/2021 Last visit: 12/1/2022 Posts: 1 Rating:
|
Hi All, The post here is quite helpful in understanding that we can use normal UR2 rack for S7-400H. We have been using UR2H in most of our projects with S7-400H since both CPU's are housed in the same panel.. There is a new requirement in our project to shift one of the CPU in S7400H system to another panel which is few 100 metres away. There are 2 concerns on this 1. Is that ok to use 2 different rack types for this system.as started below Current panel with existing UR2H and only 1 H CPU New panel with a new UR2 rack and the other H CPU. 2. Is that ok to retain the old Hardware configuration with only UR2H rack ? We believe the configuration of racks doesnt need to match with the actual rack except for the number of slots. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/11/2022 10:34:25New subject after splitting |
|
Follow us on