Industry Online Support
Technical Forum
2/18/2010 10:13 PM | |
Joined: 3/14/2008 Last visit: 12/3/2024 Posts: 2144 Rating: (964) |
your topic title will lure many people to this post. I'm not sure, but you have to do something with MPI connection to your OS station. You have to disable the IE interface and put a MPI connection instead (in hardwareconfig). Also, on the OS you have to define also MPI connection..->the os must be aware of a mpi connection. |
If I could help you, you can use the RATE button. Thank you. |
|
2/19/2010 1:12 PM | |
Joined: 4/5/2006 Last visit: 12/3/2024 Posts: 917 Rating: (63) |
Hi AhmedFM , yes, it possible to test project with PLCSIM, simple modification need likeOrecasaid. In according with your PLCSIM version you have to use MPI (PLCSIM v5.3) or Ethernet connection also (PLCSIM v5.4) during OS compile select the right network (you need put MPI card on PC station if you need it) here a link with basic steps to use it How do you use S7-PLCSIM with SIMATIC PCS 7? hope can help regards |
2/19/2010 9:16 PM | |
Posts: 43 Rating: (0) |
Dear Oreca: thank you. i will help you by posting a pic on my project. but i will post it tomorrow beacause i am working in afactory. wait my pic. regards, |
2/19/2010 9:19 PM | |
Posts: 43 Rating: (0) |
Dear CBo i will help you by posting a pic on my project so you can help me. just wait my pic. regards |
Follow us on