12/14/2023 8:43 AM | |
Joined: 12/11/2023 Last visit: 4/12/2024 Posts: 16 Rating: (0) |
Another question I have is if it's possible to create a system that reaches a certain rpm in a certain amount of time. This is the system I wanted to create, and I was wondering if it's possible to use decimal numbers. I can't see how to do it; perhaps by using a timer, but I'm not sure how. Can you help me with this problem in addition to the others? Thank you very much. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/18/2023 08:06:38New subject after splitting |
|
12/18/2023 2:41 PM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33346 Rating: (4137)
|
If I understand you correctly: Do you want to be able to adjust the speed by ± 1 revolution per minute? |
12/18/2023 2:59 PM | |
Joined: 12/11/2023 Last visit: 4/12/2024 Posts: 16 Rating: (0) |
yes it is this |
Last edited by: french guys at: 12/18/2023 15:00:03 |
|
12/18/2023 3:08 PM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33346 Rating: (4137)
|
I don't think that's possible... |
Follow us on