7/16/2018 11:03 AM | |
Joined: 11/16/2007 Last visit: 5/5/2024 Posts: 15 Rating: (0) |
TIBI68, is it possible to use Modbus Master CP340 with the CPU firmware V1, that doesn't support SFB52 and SFB53 (which FB2 and FB3 from the CP's library are using)? Would it be possible to recompile Your code to use FB102 and FB103 instead?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/16/2018 1:08:27 PMNew subject after splitting |
|
7/21/2018 10:24 AM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
As requsted. I dont have the hardware for testing. Good Luck AttachmentMBMA340_OLD.zip (29 Downloads) |
Give us your feedback and show us your respect! |
|
Follow us on