5/24/2023 11:04 AM | |
Joined: 3/27/2012 Last visit: 10/18/2024 Posts: 179 Rating: (4) |
Answer is NO This one is designed for Profinet only... |
Last edited by: Ahoora - Jafari at: 05/24/2023 13:16:57 |
|
5/24/2023 12:24 PM | |
Joined: 10/11/2006 Last visit: 10/18/2024 Posts: 5925 Rating: (810)
|
Hello, you can use the basic positioner and Onboard I/O's., but it is not designed for standalone operation. 4.3 Control/status interface - X8 5.3 Commissioning in basic positioner control mode (EPOS) The following takes the EJOG function for example to describe the commissioning in .. 7.2 Basic positioner (EPOS) https://support.industry.siemens.com/cs/ww/en/view/109810936 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on