12/13/2018 6:27 PM | |
Posts: 3 Rating:
|
But is it possible use PTO Outputs without 6ES7553-1AA00-0AB0 module with a CPU 1500?, i can´t use the PLC Open motion with "telegram3" without described card. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/14/2018 11:36:07 AMNew subject after splitting |
|
12/17/2018 7:11 AM | |
Joined: 4/28/2015 Last visit: 4/7/2025 Posts: 398 Rating:
|
Hello, there is a new ET200 SP module you could use:
The module you need: ET200S, El-Mod., 1 STEP 5V/204KHz SIMATIC DP, Electronics module for ET 200S, 1 STEP 5 V/204 kHz for stepper motor positioning 15 mm wide, 1-channel +/-5 V interface to power unit Otherwise you could you the COMPACT module of S7-1500, for example S7-1511C or S7-1512C: CPU 1511C-1 PN, 175 KB Prog, 1 MB Data SIMATIC S7-1500 Compact CPU CPU 1511C-1PN, central processing unit with working memory 175 KB for program and 1 MB for data, 16 digital inputs, 16 digital outputs, 5 analog inputs, 2 analog outputs, 6 high speed counters, 4 high speed outputs for PTO/PWM/frequency output 1. interface: PROFINET IRT with 2 port switch, 60 NS bit-performance, incl. front connector push-in, SIMATIC memory card necessary CPU 1512C-1 PN, 250 KB Prog, 1 MB Data SIMATIC S7-1500 Compact CPU CPU 1512C-1 PN, central processing unit with working memory 250 KB for program and 1 MB for data, 32 digital inputs, 32 digital outputs, 5 analog inputs, 2 analog outputs, 6 high speed counters, 4 high speed outputs for PTO/PWM/frequency output 1. interface: PROFINET IRT with 2 port switch, 48 NS bit-performance, incl. front connector push-in, SIMATIC memory card necessary
|
Follow us on