2/21/2011 7:10 AM | |
Posts: 1 Rating: (0) |
Hi TechTeam, I know that I am replying to an old post but I would like to know if there has been a change with the type of encoder permitted with the safety functions, I intend to use SLS. Is it still the case that the only type of encoder allowed is 1Vpp sin/cos with SMC20 and not HTL with SMC30? Best Regards, Ian Splitted from Sinamics S120 Safe Stop 2. |
Last edited by: O_Moderator at: 2/22/2011 8:22 AMnew subject after splitting |
|
9/27/2023 7:31 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7952 Rating: (162) |
New question published by Almen123 is split to a separate thread with the subject Is Leine-Linde FSI 862 suitable to be used as single encoder with SMC30 for SLS and SOS monitoring. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on