6/20/2023 9:42 AM | |
Joined: 12/3/2019 Last visit: 6/21/2023 Posts: 2 Rating: (0) |
I have a similar problem but that it says it is not a LAD diagram, even though it is saved with the correct .lld file extension, and it was programed and saved in Logosoft comfort v8.3. I tried renaming it, tried saving and opening from my desktop but still no joy. I tried opening opening it directly from my desktop, it opened in Logosoft but then stopped and gave the same error message, I then opened Lgogsoft and tried opening the file from within logosoft but to no avail. EDIT: attached is the file in zip format as requested. AttachmentLogo prog hwgta.zip (336 Downloads) |
Last edited by: DiscoUK at: 06/20/2023 15:37:26 |
|
6/20/2023 3:38 PM | |
Joined: 12/3/2019 Last visit: 6/21/2023 Posts: 2 Rating: (0) |
I have attached it to my original post, hope that ok? Ill add it here just in case.
AttachmentLogo prog hwgta.zip (399 Downloads) |
6/20/2023 4:13 PM | |
Joined: 12/18/2014 Last visit: 8/4/2024 Posts: 33487 Rating: (4160)
|
I think the program is damaged. Please start a Support Request to ask Siemens if Siemens can restore the program. |
This contribution was helpful to1 thankful Users |
Follow us on