8/6/2020 8:17 AM | |
Posts: 59 Rating: (9) |
https://support.industry.siemens.com/tf/ww/en/postattachments/imagecontainer/?attachmentId=113042 |
8/6/2020 8:31 AM | |
Posts: 59 Rating: (9) |
Might be, just my 2 cents, the list is made up prior to Redundant System of 1500 (R/H). And as far as I assume, the S7 1500 not suite for Chemical and Petrochemical is because they don't compliant within G3 coating requirement. Siemens Normal modules as per attachement showing all S7-300, S7-400, ET200M, ET200S, and ET200iSP modules are approved for implentation with high concentration of corrossive gas in compliance with ISA-S71.04 severity level G1;G2;G3. AttachmentISA compliance.pdf (185 Downloads) |
Follow us on