4/13/2011 1:50 AM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046) |
Hello CC2 blame Siemens for the misunderstandingas their naming conventionfor the new TIA Portal related Step 7 are (possibly deliberately?) a source ofconfusion. TIA Portal related Step 7 (current - or just about to be released - Version is V11) is called either: - (TIA Portal) Step 7 Basicor - (TIA Portal) Step 7 Professional The "traditional" Step 7 (aka Simatic Manager, V5.5 is the current version) is alsoavailable as either: - Step 7 Basis(with LAD/FBD/STL included)or - Step 7 Professional (with LAD/FBD/STL,SCL,S7 Graph and PLCSIM included) I hope this helps |
Last edited by: fritz at: 4/13/2011 1:51 AMCheers |
|
This contribution was helpful to1 thankful Users |
4/13/2011 9:40 AM | |
Posts: 6 Rating: (0) |
Fritz many thanks for this. As we say in the UK " it was as clear as mud! " before your post. CC2 |
This contribution was helpful to1 thankful Users |
4/14/2011 2:09 PM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046) |
Hello Robster the basis for the confusion is due toSiemens basically applying the same naming convention to TIA Portal related Step 7 as they already had for the "traditional" Step 7. There is method behind the madness though (I think) as TIA Portal which eventually be be the only available Step 7 (give it 5 to 7 years I'd say, but I am purely guessing here). Anyway, the "traditional" Step 7 does definetely also exist under the name of "Step 7 Basis" even though it was rarely evercalled thatby anyone (you would havesimply called it "Step 7" and made the distinction to the more powerful version by calling it "Step 7 Professional"). Don't take my word for it though, attached is the extract from the Brochure that caused CC2'sconfusion and I hope this helps.
AttachmentStep 7 Basis (from Simatic Industrial Software Brochure - November 2010).jpg (816 Downloads) |
Cheers |
|
4/25/2011 3:52 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
Hi,
|
Denilson Pegaia |
|
Follow us on