3/2/2023 6:52 AM | |
Joined: 1/21/2013 Last visit: 7/5/2024 Posts: 2957 Rating: (468) |
Hi tigranes-97, No, the BACK-UP BATTERY 3.6V/2.3AH F. PS405/407 is only for S7-400 CPUs respectively their power supplies. For S7-300 PLCs the Backup Battery 3.6V/min. 0.85Ah f.S7-300 is used, but only for the older PLCs with Memory Card, not Micro Memory Card. Have a look at 'What are the order numbers of the backup batteries for the various CPUs?'. Kind regards |
This contribution was helpful to3 thankful Users |
3/2/2023 7:02 AM | |
Joined: 1/17/2020 Last visit: 5/29/2024 Posts: 22 Rating: (1) |
Hello.No this battery for S400. |
3/2/2023 7:24 AM | |
Joined: 8/5/2022 Last visit: 6/26/2024 Posts: 24 Rating: (0) |
Thanks Stefan That was really helpful |
tig |
|
Follow us on