Industry Online Support
Technical Forum
2/10/2011 1:14 AM | |
Posts: 7 Rating: (0) |
The client wants me to install an EPROM. Is there a list of EPROM part numbers that are compatable with the 520C somewhere? I see some listed for the later models (525's and older), but I want to make sure they will work in a 520C. The part number that I have are : PPX2587681-8012 which is 64k x 8 Can I use other lower numbers like PPX2587681-8007 or -8005? Any help would be great. Splitted from TI520C Manual. |
Last edited by: O_Moderator at: 2/10/2011 10:51 AMnew subject after splitting |
|
2/10/2011 2:57 PM | |
Joined: 2/10/2006 Last visit: 3/21/2024 Posts: 147 Rating: (12) |
Man this is really old, don't you want to ask your client to replace this by a CTI CPU ? Attached is an extract from a catalog with Eprom Part Numbers. AttachmentEprom pert numbers.pdf (658 Downloads) |
This contribution was helpful to1 thankful Users |
2/10/2011 2:59 PM | |
Joined: 2/10/2006 Last visit: 3/21/2024 Posts: 147 Rating: (12) |
Attached the chapter from the 520C / 530C system manual about using Eproms. Some usefull comments on the first page.
Attachment520-530 EPROM.pdf (654 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on