6/9/2020 1:45 PM | |
Joined: 6/17/2014 Last visit: 10/27/2021 Posts: 77 Rating: (0) |
Hello, Is there a procedure to activate the 4g modem? I have a telit he910-d modem which seems to be recognized but when I go to iot2050setup I have an activation error on cellular-4g "could not activate connection : Activation failed : IP configuration could not be reserved (no available address, timeout, etc.) ". Thanks in advance, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/09/2020 14:06:58New subject after splitting |
|
6/19/2020 11:24 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, A colleague just managed to connect the Huawei ME909s-120p Card using this how-to -> Interface was named 'wwan0' and not 'usb0'. He then used this guide to create the configuration files. BR EDIT: If your card is recognized by iot2050setup there is a good chance that it is enough to edit this file: /etc/NetworkManager/system-connections/cellular-4g
|
Last edited by: Fe_lipe at: 06/22/2020 12:05:59 |
|
2/27/2021 11:54 AM | |
Joined: 3/12/2020 Last visit: 5/5/2024 Posts: 58 Rating: (0) |
Regarding the EDIT, is it possible to somehow check this when using the Industrial OS, that does not support iot2050setup?
|
Follow us on