4/16/2021 4:55 PM | |
Joined: 4/3/2019 Last visit: 12/14/2023 Posts: 1 Rating: (0) |
Hello, is there a way to change the version of the configured CU (and the attached drives) to another version in TIA v16? Drag&Drop the same CU from the catalogue with another version is possible, but i lose all the configurations of the CU and the configured drives. Copy&Paste the drives from the one Cu to another seems not work, or is there also a way? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/19/2021 08:07:03New subject after splitting |
|
4/16/2021 5:02 PM | |
Joined: 5/12/2006 Last visit: 9/17/2024 Posts: 22358 Rating: (3010) |
Hello, no this is not possible |
Follow us on