12/10/2021 12:02 PM | |
Joined: 12/17/2020 Last visit: 4/16/2024 Posts: 14 Rating: (0) |
There is a way to have the login popup also on PC Runtime? Now on PC, if I click the log-out button i return in the login screen. In this way there is no possibility to navigate into the system without a logged in user. The trick used in the panel, on PC does not works, because come out a popup that say "insufficient authorization". if it is no possible, there is a way to log in a user via script?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/14/2021 08:08:49New subject after splitting |
|
Follow us on