5/19/2024 7:23 PM | |
Joined: 8/18/2014 Last visit: 10/14/2024 Posts: 59 Rating: (0) |
Is there a way to modify the colors of the faceplates?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/21/2024 11:06:00New subject after splitting |
|
5/31/2024 6:52 AM | |
Joined: 1/11/2019 Last visit: 10/7/2024 Posts: 764 Rating: (151)
|
Hello Lesther, I think you change the value color in the process picture which I see in runtime. it is an block icon which is placed in some typical file, most probably with the name @PCS7TypicalsXXX.PDL where XXX is the name of library you are using. so when you compile your project, the block icon in your process picture will be replaced by the block icon in this typicals file. so all the change you do in your process picture will be deleted and replaced by the original object. you should change in the typical file. ( I think that also is not a good idea) but why do you want to change this color ?? I am sure there was a reason for providing this color to that field. may be you can take the block icon from @TemplateXXX file, place it in your process picture and make the tag connections manually. now you can change this block icon colors. SIMATIC Process Control System PCS 7 APL Style Guide |
Follow us on