4/11/2008 12:49 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hi pici_c, What do you like to know? Please explain it, so we can answer you. Best regards, Wizard |
4/14/2008 10:28 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, As mentioned before by the other users, there is a way to do it by ladderlogica, but that will cost a lot of programming and it will be not fast. So the sugestion to do it in a FUNCTIONBLOCK and call that functionblock in arung is better. There are fore low costs examples in the "Applications & Tools" part of the IA & DT pages: Addressing of an element in a field with a variable Index in FBD/LAD/STL25 units Temporary storage of the received data in a ring buffer according to the FIFO principle and pass on to the user interface50 units If you have SCL then it is a lot easier to make a FIFO and do all kind of data handling. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
4/16/2008 1:47 PM | |
Posts: 80 Rating: (2) |
Thanks dchartier! I think, your examples are decimal. Is it possible to input hexadecial or binary constant? pici_c |
Follow us on