1/15/2024 10:01 AM | |
Joined: 11/15/2022 Last visit: 1/22/2024 Posts: 4 Rating: (0) |
Hi, Is there any solution to properly use the 6 analog inputs (even a non-Siemens one) ? We really need to use the 6 AI, but we have to be able to wiring everything properly. There is no point to give the possibility to use inputs if they can't be properly connected... Thanks for your feedback, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/16/2024 08:45:43New subject after splitting |
|
1/24/2024 11:46 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, the Arduino shields out there mostly operate on 3,3 / 5V - the Siemens I/O shield operates on 24V. So depending on your voltage requirements the Arduino shields may fit or not. This one has 24V and 6 AIs. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on