Industry Online Support
Technical Forum
12/27/2012 8:02 AM | |
Posts: 18 Rating:
|
Hello everybody i have a plc s5 i want link to hmi easy view i want i know do you possible link between hmi easy view and s5 thanks |
12/27/2012 9:41 PM | |
Joined: 7/15/2008 Last visit: 7/13/2023 Posts: 382 Rating:
|
Hello saran6 As far as I remeber, a S5 PLC can not be directly connected to your HMI, but you can contact the manufacturer (www.wintek.com) and ask them. The other option you have is to use a Protocol Converter, depending onthe communication protocol you are using on the S5 PLC. For example, if you are usung the PG Interface port you can use a converter that connects the PG port and convetrs the 20 mA TTY signal to the Siemens S7-RFC1006 protocol (LAN / Ethernet). If I remeber corectly your HMI should be able to handle this protocol. You can find a conveter here: http://www.process-informatik.de/produkte/s5-lan or here: http://www.ibhsoftec.com/epages/63444704.sf/de_DE/?ObjectPath=/Shops/63444704/Categories/Produkte/Hardware/%22S5%20Schnittstellen%22 Regards / m.f.g |
Last edited by: legacy support at: 12/27/2012 9:43 PM |
|
12/29/2012 12:37 PM | |
Posts: 18 Rating:
|
hello dear thanks a lot |
Follow us on