12/3/2015 10:19 AM | |
Joined: 5/20/2015 Last visit: 4/29/2024 Posts: 216 Rating: (3) |
hello friends, Please guide me over following issue About audit trail, MY PROJECT STATUS IS AS FOLLOWING. 1) I HAVE INSTALLED LICENSE OF WINCC AUDIT. 2) WINDOW USER (USER BY WHICH I AM CURRENTLY LOGON TO WINDOW) HAS BEEN ADDED TO "Logon_Administrator" as well as " SIMATIC HMI AUDIT" THROUGH MICROSOFT MANAGEMENT CONTROL.
BUT I AM NOT GETTING LOGIN TO AUDIT DC & PV ( DOCUMENT CONTROL AND PROJECT VERSIONING).IT GIVES POP-OF "SERVER BUSY." WHEN OPENED AT EXTERNALLY FROM START OPTION OF WINDOW 4) THOUGH I AM GETTING LOGIN TO AUDIT VIEWER, IN AUDIT VIEWER WINDOW EVERYTHING IS INACTIVE (NOTHING GET EXPLORE EX. AUDIT DB AND AUDIT FILE.WHEN OPENED AT EXTERNALLY FROM START OPTION OF WINDOW 5) IN THE I HAVE CONFIGURE AUDIT VIEWER FOR WINCC RUNTIME BUT IT IS INACTIVE.
THANK YOU.. REGARDS GABBAR... ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/3/2015 5:07:55 PMNew subject after splitting Let's do it... |
|
12/5/2015 8:13 AM | |
Joined: 5/20/2015 Last visit: 4/29/2024 Posts: 216 Rating: (3) |
is there someone who can help me over above topic.... Please... thank you.. |
Let's do it... |
|
9/13/2018 5:14 PM | |
Joined: 3/22/2010 Last visit: 5/14/2024 Posts: 76 Rating: (0) |
Hello, Has anybody solved this issue? I have the same case in WinCC/Audit v7.4 SP1 Upd1 Thanks, t rk |
Follow us on