9/19/2022 7:36 PM | |
Joined: 3/17/2022 Last visit: 9/27/2023 Posts: 3 Rating: (0) |
Hi Dears, Currently I face issue when migrating PCS7 V8.1 to V9.0 SP3 with APF V2.0 to V2.1 Upd2 The issue is that the enumeration doesn’t appear on the run time in the job parameters, it was appearing before the upgrading but now it doesn’t. The declaration folder in the master library is already synchronized with the project declaration folder. Could you please support me on that. Best Regards, AttachmentPictures.zip (273 Downloads) |
9/20/2022 4:40 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, Did you do the update procedure? You need to generate the FB blocks in the APF Engineering Tool, create the archives on the OS and execute AS compile+download and OS compile+download. Please check the readme if you have followed all steps: |
Last edited by: Oreca at: 09/20/2022 04:42:11Last edited by: Jen_Moderator at: 09/20/2022 10:51:47Link optimized. If I could help you, you can use the RATE button. Thank you. |
|
9/21/2022 9:59 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, Thank you for the feedback! Great that it was solved. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on