Industry Online Support
Technical Forum
11/19/2009 6:16 PM | |
Joined: 6/5/2009 Last visit: 3/1/2024 Posts: 149 Rating: (0) |
Hi ppl, I was sent to commission a Sinamics G130 drive. The male pins in the slot responsible to host the Memory card/ license chip was bent at odd angles due to some some unknown problem. the card could not be inserted in the control unit due to this and communication could not be established. The AOP did not respond to finger touches. Am I right in guessing that the memory card is the integral piece for the functioning of the drive and the lack of proper mounting the reason for the drive failing to communicate with the field PG and for the AOP not functioning? Please help. My second issue would be familiar to that of a person not too familiar with a Sinamics drive and the Starter software. Please give me the technique of configuring the G130 drive for the inputs/ outputs that I have attached below. Please explain the control logic if any exists. Thanks a lot for the help in advance.
Attachment11 AMB DR.TM31 Model.pdf (392 Downloads) |
11/20/2009 5:59 PM | |
Joined: 6/5/2009 Last visit: 3/1/2024 Posts: 149 Rating: (0) |
DearDrives_Coach, Thanks a lot for the reply and there is the second part that I need some help. This is about configuration of a Sinamics G130 drive based on the diagram given in the first post. Please let me know if there are any materials(documents) that I could refer for the configuration/ commissioning of the drive by using the field PG. Thanks a lot.
|
Follow us on