4/28/2020 12:19 PM | |
Posts: 2 Rating: (0) |
Hi all I have a problem with two counters I'm using to update the on / off values of a threshold trigger, using the arrow keys on the TD. But because the CNT value in the parameter box isn't updating it's not allowing me to change the threshold trigger parameter values. The analogue threshold trigger is looking at a pt100 sensor, the program is the start of a heating control system. Cheers AttachmentHEATING TEST V1.zip (99 Downloads) |
Follow us on