6/29/2021 6:03 AM | |
Joined: 3/31/2018 Last visit: 11/25/2023 Posts: 8 Rating:
|
Hi Vishnu, I'm Facing the same issue with one of my client, for my CPU 1510sp-1pn Module.. I tried all stuffs by removing all IO cards, and kept only one DI module with server module at last. After doing multiple power recycles, I decided to go with one DI module for rectification. Another one information that there is a mismatch with the firmware like it was configured as v1.0.8 in Hardware config & physically CPU has v2.0.1. Please help me to overcome this issue. Experts also kindly note that it was running since 2017 till last month.. So Vishnu, can you please update how did you overcome this issue.. ? Regards, Haresh KM ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/29/2021 06:10:27New subject after splitting Regards - Haresh KM |
|
Follow us on