7/31/2023 9:31 AM | |
Joined: 6/4/2018 Last visit: 7/8/2024 Posts: 2 Rating: (0) |
We are facing significant issues with starting the WinCC Runtime, as it occurs more frequently. A Reset_WinCC.vbs is definitely not the solution. WinCC RT Professional V17.0 Upd5 OS: Windows Server 2019 Standard The only solution is to delete the project folder and reload WinCC onto the system via ES (Engineering System) again (for a redundant system, this is an increased effort). What is the solution here? Can the error be avoided or resolved more quickly? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/31/2023 10:27:08New subject after splitting |
|
Follow us on