1/11/2023 4:45 PM | |
Joined: 5/26/2017 Last visit: 1/13/2023 Posts: 3 Rating: (0) |
Hi, I´m also having issues with the battery backup of the RTC. Currently finishing a project with 20 LOGO units, (12/24 RCE, 6ED1052-1MD08-0BA1). Initially no of the units was working regarding the backup of RTC after power down, after trying with 24h power on, 3 units is now "fixed" and keeping time after power down..... Does any one know if there is a battery, or a capacitor inside the unit for RTC-backup? Makes no sense if you have to charge a RTC-backup battery for more than 24h before it starts working properly! Leaving the rest of the units to bake an additional 24h before call it quits on this. ------------------------------------------------------------------------------------------ |
Last edited by: mr steel at: 01/11/2023 16:50:27Last edited by: Jen_Moderator at: 01/12/2023 08:26:50New subject after splitting |
|
1/11/2023 4:59 PM | |
Joined: 12/18/2014 Last visit: 7/18/2024 Posts: 33367 Rating: (4138)
|
The LOGO! has no Backup Batterie but a SuperCap. |
Follow us on