Industry Online Support
Technical Forum
7/3/2024 1:00 PM | |
Joined: 6/26/2024 Last visit: 7/5/2024 Posts: 1 Rating: (0) |
Dear Siemens Support Team, I am writing to seek your assistance with an issue I am encountering while trying to update and integrate software packages in SIMATIC Manager. Issue Description: I am attempting to update S7 V5.7 with the project 'SW/Latvia20230523', but I am facing issues due to missing or outdated software packages. I have identified that the following components need to be updated or integrated: Drive ES / SIMOTION PDM (Process Device Manager) SIMATIC WinCC Flexible SIMOTION However, I am unsure of the exact steps to properly integrate these packages into SIMATIC Manager. I have tried the following steps without success: Open SIMATIC Manager. Navigated to 'Options' > 'Customize...'. Attempted to add the necessary software packages under the 'Packages' tab. Request: I would appreciate detailed guidance on the following: How to properly integrate the required software packages into SIMATIC Manager. Any specific steps or configurations needed to resolve the missing package issue. Information on ensuring all components are up-to-date and compatible. Please let me know if you require any additional information from my side to assist with this issue. Thank you for your support. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 07/03/2024 13:01:29New subject after splitting |
|
7/3/2024 2:16 PM | |
Joined: 5/6/2022 Last visit: 7/24/2024 Posts: 434 Rating: (84) |
Hi AutoGen_3483510, If in the project you are trying to open you want to continue working with the components it requests (Simotion, PDM, etc.), you will have to acquire these components and install them on your PC. They are packages that have a license associated with them. To check the versions compatible with Step 7 V5.7 you must consult the compatibility tool: If you do not have to use these components you can delete their information from the project, in the "File" option - "Save as" - and select the "Slow Reorganization" option from the Siamtic Manager. Best regards!
|
Last edited by: Wit_Moderator at: 07/04/2024 13:43:46Link optimized If this Information really helps, you could use the Rate function |
|
Follow us on