4/8/2015 7:10 AM | |
Joined: 6/27/2008 Last visit: 7/6/2021 Posts: 43 Rating: (4) |
No, you must use different IP's for redundant OS servers. |
4/8/2015 8:29 AM | |
Posts: 567 Rating: (107) |
Hi, as you can read before it is not possible to have the same IP addresses. To get some more information about how to setup a PCS 7 project in general (AS, OS, clients) you should have a look in the PCS 7 compendium. This is a very good guideline will answer a lot questions You can find it under the following link: |
4/8/2015 11:42 AM | |
Posts: 4 Rating: (0) |
Different IP and MAC for redundant AS CP's. |
Follow us on