8/31/2017 9:05 AM | |
Joined: 4/3/2017 Last visit: 6/1/2023 Posts: 6 Rating: (0) |
Hiii, It is possible to upgrade S71200 cpu1214dc/dc/dc v2.2 into v4.1 ? it is possible means please post the update file. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/31/2017 1:03:35 PMNew subject after splitting |
|
8/31/2017 9:22 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
no, thats not possible. S7-1200 CPU´s of the 1st generation (e.g. 6ES7214-1AE30-0XB0 ) can be upgraded until FW-V2.2 S7-1200 CPU´s of the 2nd generation (e.g.6ES7214-1AG31-0XB0 ) can be upgraded until FW-V3.x S7-1200 CPU´s of the 3rd generation, the actual generation (e.g.6ES7 215-1AG40-0XB0 ) starting with FW 4.x hope this helps, regards, The actual S7-1200 CPU are coming with FW 4.2 and are only projectable in Step7 V14. |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on