2/29/2012 12:37 PM | |
Posts: 23 Rating: (3) |
Dear lambertws, It is better to use the normal jump operations than the system opearatiopns. In the manual it is very good described, please refer to the attachment. It is time to say good bye to S5 because the live time end is near. Please refer also to http://support.automation.siemens.com/WW/view/en/13266996 Attachmentpages from_PA928B_JUR.pdf (90 Downloads) |
Last edited by: rosi at: 2/29/2012 12:37 PM |
|
3/6/2012 9:37 AM | |
Posts: 23 Rating: (3) |
Dear lambertws As BeVeeanswered and my screen shot before here an additional screen shot from STEP 5 with your operations. |
This contribution was helpful to1 thankful Users |
3/7/2012 3:39 PM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating: (90) |
Hi lambertws, I did some tests. Testreport and screenshots in attachment. But as I said before, you won't need this block in converted program. Better use S7 PID blocks. Kind regards, BV AttachmentJUR.zip (96 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on