2/10/2022 9:11 PM | |
Posts: 257 Rating: (77)
|
Hello SIOS Forum Community, this post will illustrate how to protect data on the SIMATIC S7-1200/S7-1500. It should be noted that there are different possibilities that cover different use scenarios. These possibilities can be combined to cover the desired use cases. Protection of devices There are 3 options for protecting building blocks:
Further information can be found in the TIA Portal manual. Protection against access to the CPU To restrict access to the CPU, the access level can be set during configuration. The following access levels are available:
Further information can be found under the following link: Notes: The parameterised access levels do not provide high-quality protection against changes to the programme. It is possible to change the programme via the memory card. To prevent this, the access protection must be combined with the know-how protection. In a protection concept, the OPC UA server and the web server of the control system should be taken into account. Further information can be found in the following links:
The information described in this article refers to the time of writing this article (status: June 2021). Your sincerelly SIMATIC International Technical Support Hub |
This contribution was helpful to4 thankful Users |
Follow us on