12/23/2014 11:52 AM | |
Joined: 1/28/2009 Last visit: 4/22/2025 Posts: 6867 Rating:
|
You can try migration tool independently as explained in the following link: Download Migration Tool
But it still has the installation limitation over older operating systems. |
6/15/2015 9:14 AM | |
Posts: 9 Rating:
|
I managed to remove "know how protection" from KNX blocks in TIA v13. Now there is new problem. Blocks are programmed for Step7 so they seems to be incompatible for TIA and compilation shows multiple errors. They have to be checked and changed to TIA standard so they can be compiled. As I found some other solution for my problem I dismissed KNX completely. I attached converted and unlocked blocks I have for TIA portal so if anyone wants to work on them is free to do so. If someone manages to get these block working it would be nice to share this with others.
AttachmentKNXTest_V13_SP1.zip (185 Downloads) |
6/15/2015 9:16 AM | |
Posts: 9 Rating:
|
Second part of the zip. Rename this file to KNXTest_V13_SP1.z01 in order to unpack files. I could not upload .z01 file. AttachmentKNXTest_V13_SP1.zip (188 Downloads) |
1/18/2016 8:12 AM | |
Posts: 1 Rating:
|
i unable to open it how to open it in tia. when i open it in tia i face general input/output data error |
Last edited by: dknjsingh at: 1/18/2016 8:17:49 AM |
|
Follow us on