9/12/2018 4:11 PM | |
Joined: 3/27/2012 Last visit: 6/9/2023 Posts: 32 Rating: (10) |
If they have an ability to load project (corresponding interfaces), then Pack'n'Go will help you. Make changes in your project and then use pack and go. Pack and go is the utility that builds a package of project loading tool and project files, so the project can be loaded without TIA Portal (there was similar functionality for wcc flexible in the past). |
10/23/2021 6:52 AM | |
Joined: 4/23/2014 Last visit: 8/20/2024 Posts: 4 Rating: (0) |
I read it's manual, it seem cannot change by local. |
10/23/2021 10:34 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hi, There are two ways:
|
Ayman Elotaify |
|
Follow us on