1/28/2022 8:32 AM | |
Joined: 4/24/2006 Last visit: 10/3/2024 Posts: 8744 Rating: (1168)
|
Hello, What is the version of TIA Portal you are using? Can you check the image version of your panel in the project? (Properties of panel, general information) Sm@rtserver is possible when you use TIA Portal v14 or higher, and the image of v14 or higher Best regards, Wizard |
This contribution was helpful to1 thankful Users |
2/2/2022 1:01 PM | |
Joined: 8/3/2009 Last visit: 10/2/2024 Posts: 13831 Rating: (1745)
|
Hello if you have transfered the correct image to the Panel then you can see also the settings in Control Panel: https://support.industry.siemens.com/cs/de/en/view/90114350/143297380107 It will work also without License for testing purposes but you will get always a license message. So for productive work you need a License on the Panel. If you work with TIAPortal V17 (and V17 Image) then you do not need a License any more. The functionality then is included for free also for Basic PAnels 2nd Gen. Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/7/2022 1:38 PM | |
Joined: 8/3/2009 Last visit: 10/2/2024 Posts: 13831 Rating: (1745)
|
Hello yes I am sure, you can read it in the manual: https://support.industry.siemens.com/cs/de/en/view/90114350/143297380107 And also i have tested it, ther is no license message any more if you use it without license on the Basic 2nd Gen in V17. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on