6/30/2017 2:09 PM | |
Posts: 2 Rating:
|
Hello, I successfully connected a KTP 400 basic to a Siemens Logo8.FS4. Everything works fine with Network Signals and analog Signals to he KTP and Digital Signals from the KTP. One thing I could not figure out is how to Map a digital output from the Logo to the KTP. The problem is that I want to use the network output from the Logo to crate an event which illuminates a circle on the KTP screen when according to the status of an inductive sensor. I hooe someone can help me. AttachmentLogo Tia.zip (149 Downloads) |
Last edited by: 123+asd at: 6/30/2017 2:13:09 PM |
|
6/30/2017 2:34 PM | |
Joined: 12/18/2014 Last visit: 8/25/2024 Posts: 33616 Rating:
|
The state of digital outputs is determined by the operating system of the LOGO! In firmly allocated areas in the VM area. Example: AttachmentLOGO! 8 Soft Comfort Online-help 2016_07 (FS4) page 114.pdf (183 Downloads) |
7/3/2017 7:59 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating:
|
|
Last edited by: Jen_Moderator at: 7/3/2017 1:58:47 PMMy Forum is the place to personalize your profile, |
|
This contribution was helpful to
1 thankful Users |
Follow us on