12/31/2017 3:51 PM | |
Joined: 3/20/2017 Last visit: 11/8/2024 Posts: 143 Rating:
|
Is it possible to use both Modbus TCP and ProfiNET in the KTP1200 basic panel (in the same time)? |
1/1/2018 12:21 PM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, this is not possible probably. Profinet port can be used in your case for S7-1200 connection f.ex. and can't be shared. If your HMI has also RS-422/485 serial port this can be used as MB RTU channel. In case of your MB Server has only TCP protocol, suitable Gateway MB RTU-TCP can be used to solve this problem. Everytime look for first to your HMI order number documentation, system info for proper informations about intefaces, protocols. Update: to be clear, in case you want use your HMI Profinet port with MB TCP and it support this, you can use that of course, but share that 2 protocols via one Profinet port is not available. You can also simply prepare your cfg in WinCC and there you can create your cfg and see what you can do. |
Last edited by: Duris_I at: 1/1/2018 12:23:12 PMLast edited by: Duris_I at: 1/1/2018 1:16:11 PMWith best regards... |
|
Follow us on