9/16/2013 8:15 AM | |
Posts: 461 Rating:
|
Create a PN/IE interface for downlaoding ... C this link , here while downloading PN/IE interface was selected ...In ur Hardware configuration -> Device view,right click ur ethernet port & create PN/IE interface & while downloaidng select it from the PG/PC interface .. it will lead u to donwload... Regards, Nelliyan.G |
5/26/2014 11:43 AM | |
Posts: 163 Rating:
|
Hi, I have the same problem. ![]() Can you pls send me the link for downloading HSP for KTP 400 Color PN? Rudrani |
5/26/2014 11:56 AM | |
Joined: 4/24/2006 Last visit: 3/16/2023 Posts: 8586 Rating:
|
Hello Rudrani, Have a look at the following link: hardware support packages (HSPs) for WinCC (TIA Portal) Best regards, Wizard |
Last edited by: Wizard at: 5/26/2014 11:56 AM |
|
This contribution was helpful to
1 thankful Users |
9/10/2015 11:06 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4827 Rating:
|
New question published by SAT_BAR287 is split to a separate thread with the subject KTP400 basic pn TIA portal v11, hardware configuration don't show panel. Best regards |
1/28/2016 3:59 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4827 Rating:
|
New question published by ta_sonnet@yahoo.com is split to a separate thread with the subject KTP 400 Mono PN, touch cannot be calibrate. Best regards |
Follow us on