5/10/2019 7:16 AM | |
Joined: 9/12/2016 Last visit: 6/26/2022 Posts: 17 Rating: (0) |
THE SAME PROBLEM WAS SOLVED IN THE TOPIC "Converting one HMI OP177B which is communicating to D445BUT,HERE PHYSICAL SIMOTION CONTROLLER FIRMWARE WAS CHANGED. I HAVE APROBLEM THAT IN STEP7 HARDWARE I CANNOT FIND D445-FIRMWARE V4.3. HOW CAN I GET D445-FIRMWARE V4.3 IN HARDWARE CATALOGUE SO THAT I CAN CHANGE IN THE STEP7 AND CAN INITIALZIE DEVICE PROXY ------------------------------------------------------------------------------------------ |
Last edited by: kanchan14 at: 05/10/2019 07:19:27Last edited by: Jen_Moderator at: 05/10/2019 11:39:52New subject after splitting Last edited by: Jen_Moderator at: 05/10/2019 11:40:06New subject after splitting Last edited by: Jen_Moderator at: 05/10/2019 11:52:11Optimized splitting remark. |
|
5/10/2019 11:46 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject How can KTP700 communicate with D445? is published within the conference Motion Control System SIMOTION. Best regards Jen_Moderator |
Follow us on