10/15/2019 11:38 PM | |
Joined: 7/2/2019 Last visit: 3/24/2021 Posts: 9 Rating: (0) |
Hello there, My HMI is KTP900 Basic PN. I can't find "ExportDataRecords" system function under events. Any help appreciated. Regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/16/2019 12:18:56New subject after splitting |
|
10/18/2019 6:15 AM | |
Joined: 7/5/2013 Last visit: 7/18/2024 Posts: 3107 Rating: (509) |
Hello ekeyfoglu,
ExportDataRecords is a system function that can be called with one of the events. Select one of the events and then <Add function> on the right. Possible to add the named function e.g. when screen loaded, when button pressed, when value of tag changed. Regards, Frink |
Pi is exactly three! |
|
Follow us on