8/23/2023 8:48 AM | |
Joined: 2/17/2020 Last visit: 7/16/2024 Posts: 1022 Rating:
|
Hi, I'm afraid it's a hardware limit of the HMI model used, as detailed in the manual: Scope of functions with WinCC - Recipe - Elements per recipe However, when arrays are used, each array element represents a recipe element, so maybe you can take advantage of that. |
A rating will be well appreciated. |
|
8/29/2023 11:17 AM | |
Joined: 8/3/2009 Last visit: 7/17/2024 Posts: 13308 Rating:
|
Hello this is not 100% correct in case of a recipe every array element counts like a single element. https://support.industry.siemens.com/cs/ww/en/view/109815056/149330043275 (Check the footnote...) Unfortunately the Basic Panels are limited so you cannot use such big recepies. Comfort Panels can handle more recipe elements (you can find in the system limits in the link above) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on