5/31/2018 4:18 PM | |
Posts: 2826 Rating:
|
Hello.
You did not mention for which device you are asking about. To start the discussion I have designed code in SCL for the S7-1200. Included is a text file that can be imported into TIA to make an FB. Also is a timing graph with simulated run. Focus on the core idea and see if you can develop your LAD code from this working sample.
BR Attachmentgenerate 3 pulses.zip (39 Downloads) |
Last edited by: #dP at: 5/31/2018 4:46:05 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on