5/21/2010 8:16 AM | |
Joined: 10/7/2005 Last visit: 6/2/2024 Posts: 3007 Rating: (1049) |
Hello sun7 I think you are out of luck here and will have to manually program the CFC logic to do what the original LAD/FBD/STL logic did. Even though CFC does "compiles down"into STL (via an intermittent SCL step for that matter), and LAD/FBD areessentially STL displayed in graphical form, the reverse "up compilation" of LAD/FBD/STLinto CFC charts is not possible (well at least not with any inbuilt availableStep 7tools that I am aware of). I hope this helps anyhow |
Cheers |
|
6/2/2010 3:11 AM | |
Joined: 5/28/2008 Last visit: 5/29/2024 Posts: 4507 Rating: (837)
|
Welcome sun7, Please have a look on the following link: http://support.automation.siemens.com/WW/view/en/34008480 Then download the section of "7. Graphic Programming with the CFC-Editor" It's very helpful. Enjoy it. |
Last edited by: Ayman Elotaify at: 6/2/2010 3:15 AMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
Follow us on