7/20/2016 2:52 PM | |
Joined: 8/25/2014 Last visit: 4/19/2024 Posts: 133 Rating: (1) |
This is a little bit off topic but still. I have a problem with language switching in my latest project. In the language and resources/Project languages I have defined two languages. Slovenian and Serbian and I have removed the english language. Both the Editing and reference language is set to Slovenian. But If I try to switch between these two languages via a on screen button I can't do it. If instead of toggle I try to define a certain language, only Serbian is an option, no Slovenian. What could be wrong? Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/21/2016 12:30:51 PMNew subject after splitting |
|
2/1/2020 7:23 PM | |
Joined: 9/3/2018 Last visit: 6/9/2023 Posts: 29 Rating: (0) |
Thanks Polijo.I had the same issue |
Follow us on