10/10/2016 3:08 PM | |
Joined: 4/28/2015 Last visit: 11/12/2024 Posts: 3345 Rating:
|
You can download the latest SD-Card Example Image here: How the SIMATIC IOT2000 can be put into operation with the SD-Card Example Image please refer to "Setting up the SIMATIC IOT2000". On the download page you can find also the Open Source Software ("OSS") and the Readme-OSS. Hint: This image is valid as of the release hardware of all SIMATIC IOT2020/2040. Tools you will need to operate with the SIMATIC IOT2000:
---------------------17.06.2021--------------------- new features / fixes / improvements in V3.1.1
- updated CIP 4.4 kernel - updated to Node RED 1.2.1 - updated pre-installed nodes - security-fixed Node.js 8.17 - accelerated boot in low-entropy scenarios - improved booting from external media (USB sticks etc.) ---------------------14.07.2020--------------------- new features / fixes / improvements in V2.6.1 - Update to Yocto 2.6 (thud) - Update to nodejs 8 - node-red-contrib-mindconnect, node-red-contrib-iiot-opcua, and node-red-contrib-modbus preinstalled - Prepare over-the-air updates via SWUpdate (requires customized image) - Add timezone configuration support to iot2000setup - workaround for installing node-red-nodes (as with 2.6.0) not required anymore - Various updates and cleanups ---------------------27.06.2019--------------------- new features / fixes / improvements in V2.4.0 - Yocto Rocko (V2.4) - CIP kernel 4.4.154-cip28/-rt20 - Enable peripherals menu on IOT2020 - Fix DHCP in the presence of connman - Enable Realtek RTL8XXX wireless LAN driver - NodeJS v6.14.3 - Added python3-setuptools and python3-lxml - And more!
new features / fixes / improvements in V2.2.0 - Linux Cip Kernel 4.4.105 - Yocto 2.2 (Morty) - Nodejs v6.12.3 - Mosquitto 1.4.14 - Python V2.7.12-r1 - Python3 V3.5.2 - Swap File support (extending RAM) ---------------------19.04.2017--------------------- new features in V2.1.3 - Nodejs v6.9.2 - Mosquitto commandline tools - Pip and python3 modules - File system is expanded at first boot now (please be patient - first boot will last a few minutes due to this) fixes/improvements in V2.1.3 - iot2000setup script improved - node-red issue fixed (starting node-red manually or per autostart will not influence the working directory --> will always be /home/root) ---------------------19.12.2016--------------------- new features in V2.1.2 - npm included in the image - node-red preinstalled - included packages: lsusb, resize2fs, wireless-tools, tree, i2c-tools, sqlite3 - setup script for common tasks (set ip address, hostame etc...) - mraa version 1.5.1 - some firmware files (realtek and broadcom) for usb wifi sticks added - second LED (H6) in IOT2040 is now supported under /sys/class/leds fixes: - load i2c-dev at startup - some parts in the readme were extended - mraa import in python works now |
Last edited by: bergmanu at: 12/19/2016 9:21:04 AMnotes V2.1.2 Last edited by: bergmanu at: 4/19/2017 10:04:31 AMnotes V2.1.3 added Last edited by: bergmanu at: 4/19/2017 10:04:47 AMLast edited by: bergmanu at: 8/9/2017 5:55:55 PMadded links top software Last edited by: bergmanu at: 4/13/2018 1:15:30 PMLast edited by: bergmanu at: 06/27/2019 07:56:02added V2.4 Last edited by: bergmanu at: 04/29/2020 09:13:27changed all IOT2000 to IOT2020/2040 Last edited by: bergmanu at: 05/06/2021 13:05:27added V2.6.1 Last edited by: bergmanu at: 06/17/2021 15:18:52Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
3 thankful Users |
11/13/2016 1:04 PM | |
Posts: 1 Rating:
|
Seems that a PHD or or higher is required to download the SD-Card image. I successfully registered, got authorized to download export restricted software but this doesn't seem to include export to countries next go Germany,.. Unfortunately, an automated release of the desired download via the Web is not possible. That does not mean that the download is excluded. You can now forward the process for manual checking.
|
11/14/2016 7:43 PM | |
Posts: 30 Rating:
|
I get the following: You cannot download this file, since you do not have the necessary authorization yet. Your registration inquiry will now be forwarded; due to the manual review the registration may take several days, however. You will get a confirmation e-mail as soon as your download registration is finalized. You can download the requested software or other software packages only when you have received the positive confirmation. Why is this here? Not helping yourselves by making it non-user-friendly to download the software needed to make this thing work... |
11/14/2016 8:00 PM | |
Posts: 30 Rating:
|
Apparently you can get everything you need here to compile your own image: https://github.com/siemens/meta-iot2000 I may compile the minimal and example images tonight, and put them up on Dropbox for others. |
11/16/2016 8:00 AM | |
Joined: 4/28/2015 Last visit: 11/12/2024 Posts: 3345 Rating:
|
Sorry for this long process in order to download the example image. But this is necessary due to export restrictions. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/16/2016 4:07 PM | |
Posts: 1 Rating:
|
Today i got my IOT2020 and i can't wait to start developing. But i'm not authorized to download the SD Card Image even i registered myself 3 days ago. Pretty disappointing and i can not understand this problem. Who at Siemens can tell me how long i still have to wait until i get the necessary permission ? |
Last edited by: Min_Moderator at: 11/17/2016 12:29:30 PMNew subject after splitting Last edited by: Min_Moderator at: 11/17/2016 3:46:08 PMMoved back |
|
11/16/2016 5:57 PM | |
Posts: 30 Rating:
|
If I compile the image source located here: https://github.com/siemens/meta-iot2000/tree/master/meta-iot2000-example and post a link to the resulting wic image, would that be acceptable? |
11/17/2016 4:06 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
Hello mobilefirst, the authorization process can take up to seven days. You will be informed by Email if the process is finished. |
This contribution was helpful to
1 thankful Users |
11/23/2016 10:37 AM | |
Joined: 1/26/2011 Last visit: 11/12/2024 Posts: 243 Rating:
|
Hello together, after creating my account and try to download the SIMATIC IOT2000 Image it just took me up to 1 day. At the beginning I filled out my account information with one mistake (not on purpose) but after receiving an e-mail after round about 2 hours I got the information how to fill out the personal account information. For private usage you should fill out the company field and departmend field with "private usage" or in German "private Nutzung". All in One I can tell you that my test was successfully finished after 1 day with permission to be able to download the latest SD Card Image for the SIMATIC IOT. I hope this information will help you.
|
12/19/2016 9:22 AM | |
Joined: 4/28/2015 Last visit: 11/12/2024 Posts: 3345 Rating:
|
Hi all, new image version V2.1.2 is now available! Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
We are working on a new user interface with better overview and more relevance.
Follow us on