8/31/2016 5:40 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
PLC watch dog has activated. Do you have step7? Connect & check diagnosis buffer. |
8/31/2016 1:00 PM | |
Posts: 25 Rating:
|
Hello As I said in my last post I have no communication with the NCU either via Step7 Simatic Manager or with HMI, have the alarm 120202. even make the reset sequence S4 (PLC) MRES-STOP STOP ("2" - "3" - "2"). I have to understand why the PF Led Blinks 8 times (PF PLC Watchdog (red), I find the manuals this information. as the NC-PLC data there is no problem data, have all the bach up Thanks Flopez Send Video https://youtu.be/QCkqyCp4Xp8 |
Last edited by: flopez at: 8/31/2016 2:59:31 PMhttps://youtu.be/QCkqyCp4Xp8 |
|
9/3/2016 12:15 AM | |
Posts: 25 Rating:
|
>Do you have good back up data for this m/c--NCK and PLC data? Yes I have all backups for this unit. >Do you have PG or PC installed STEP 7 sw. and you have communication cable? Yes have a SIMATIC FIELD PG, communications cable, SIMATIC Manager Version 5.5 software and connected to -X122 PG MPI. and have no communication with the unit and a message appears impossible Online error. (with all the correct parameters) CP5611 (MPI) 187.5Kbit / s. I am also using the Sinumerik HMI Advanced software connected to the -X101 the MPI 1,5Mbit/s and the error message with is 120202 (send attached photo) >If you like you can tell more detail why you NCU display like that. The NCU became so after a short break of 3 weeks. When I has intervened in the NCU found that this was very dirty, the backup battery circuit had broken the clues with corrosion. It was repaired total. (Condensers, fans, battery, and more) He never came out of this. Thanks for your interest in solving this big problem Flopez AttachmentHMI Advanced.pdf (112 Downloads) |
9/3/2016 8:02 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello flopez, Does your system has 2 NCUs? How are they connected? Can you attach here your system Hardware configuration? |
9/3/2016 3:10 PM | |
Posts: 25 Rating:
|
flopez |
9/3/2016 3:26 PM | |
Posts: 25 Rating:
|
Hello Already found the cause of the fault. It PLC module (570572.9202). This is because today was from a NCU to the testing of modules PLC and COM. and I found that the error is in Modulo PLC, so I can only find a piece of these I will make the breakdown of research of this module (if possible) Thanks To All Flopez Obs. When you have new news I will report here AttachmentModulo PLC.pdf (130 Downloads) |
Follow us on